Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For all CAD systems, under PARTadmin -> Category -> PARTsolutions -> CAD integration -> specific CAD system, the tabbed page AttributeMapping (3D/2D/native) is displayed. In the corresponding configuration file the respective block name is "AttributeMapping".
Note | |
---|---|
On this tabbed page normally you don't have to make extensive changes, unless you want to create another tabbed page. Especially because of this the logic of structure is described. Otherwise you control the language of PARTsolutions default attributes with the value of the "Attr_CopyFrom" key (on this see the next section under Attr_CopyFrom). |
PARTadmin -> Category -> PARTsolutions -> Configuration files -> $CADENAS_SETUP -> if<cadname>.cfg: Fig. exemplified for SolidWorks
Here you can adjust the following:
Transfer of PARTsolutions default attributes:
Shall the PARTsolutions default attributes be transferred to the CAD system?
If yes, in which language(s). (About language variants see under Section 2.2.4.5.3, “Export standard attributes in several languages ”.)
| ||||
[a] For example, if errors arise in the CAD when transferring system attributes (e.g. "Material"). |
Per default some blocks are defined, which are used to set custom attributes and in addition for some cad systems special attributes which are displayed in special dialogs in the CAD system.